Jürgen Wagenbach
- Total activity 548
- Last activity
- Member since
- Following 0 users
- Followed by 2 users
- Votes 2
- Subscriptions 408
Articles
Recent activity by Jürgen Wagenbach Sort by recent activity-
MAXPOS: Export / upload the configuration into a *.mxpj project file
Topic: How to export the parameter settings of a MAXPOS controller into a file? Situation: If you want to ... ... copy the configuration of a MAXPOS to another one, ... save the configuration as...
How to connect a cable's shielding to Earth potential?
Topic: How to connect the shielding of cable to a earth potential? Situation: All modern power stages of motor controllers use PWM voltages to control the motor supply. Such PWM power signals can r...
EPOS / IDX: Export of parameter configuration in a *.dcf file
Topic: How to export the parameters and configuration information of an EPOS4, EPOS2, or EPOS? Situation: If you want to ... ... copy the configuration of an EPOS4 (or EPOS2, EPOS) to another on...
maxon BIKEDRIVE: FAQs about the Drive Unit (Motor and Gear)
What torque does the maxon BIKEDRIVE AIR e-bike system provide? The system delivers a peak torque of around 40 Nm. How many levels of support are there? There are three levels of support. The m...
Is maxon a bicycle manufacturer?
Question: Is maxon a bicycle manufacturer? Answer: maxon does not produce bicycles, but instead is a system supplier for e-bike drives for the bicycle sector.Here you find the actual bike brands ...
Availability of data sheets of CTO motor combinations (e.g. DCX, ECX)?
Topic: Why do I not have access to the specification of a configurable drive unit (e.g. based on a DCX or ECX motor)? Solution: Any configurable (so called "CTO - Configure to Order")...
MAXPOS Studio: Download of a *.mxpj project file to a MAXPOS controller
Topic: How to import / download the parameters of a *.mxpj project file to a MAXPOS controller? Solution: The "MAXPOS Studio" software is based on a project structure to manage system and drive pa...
EPOS / IDX: Export of the *.eds resp. *.esi file (Electronic Data Sheet)
Topic: What do the abbreviations EDS / ESI mean? What is the EDS / ESI file used for? Where to find the *.eds / *.esi file of an EPOS, EPOS2, EPOS4, or MCD? Solution: The term "EDS" stands for "E...
Support Center: Issues of the former Support Desk until 2018
Topic: The former so-called "Support Desk" was replaced on Monday, 15th October 2018 by this "Support Center". All still open support issues of the fromer "Support Desk" at that time had been merge...
ESCON: Export / Upload of the configuration in an *.edc file
Topic: How to export the parameters and configuration information of an ESCON? Situation: If you want to ... ... copy the configuration of an ESCON to another one, ... save the configuration as ...