Does maxon offer a display?
No, maxon does not offer its own displays. However, maxon’s control unit can communicate with many devices, for example from Sigma, Garmin, and other providers, via BLE or ANT+.
Can I pair an external GPS device with the maxon interface?
Yes, that can be done via BLE or ANT+. Once the external device is connected, the battery display or support level can be shown on the display.
Can I connect a light to the system?
Yes, a light can be connected. However, an additional module is needed between the battery and control unit. maxon provides a 12 V output for the light (max. 10 W).
Can I adjust the luminance of the LEDs?
The LEDs automatically adapt to the lighting conditions.
Can I connect my smartphone to maxon’s interface?
Yes, with the maxon Service app (for specialist dealers) or the maxon Connect app (for end customers), you can connect a smartphone to the system, configure settings, or get a data readout.
How can I see whether my smartphone is connected?
When the blue LED on the control unit is lit, the smartphone is connected to the BIKEDRIVE AIR.
Is the Range Extender displayed when it is connected?
Yes, the Range Extender is displayed and the green LED on the interface is lit.
How is the battery capacity displayed when the Range Extender is connected to the system?
The Range Extender works like a power bank. This means that the Range Extender charges the main battery. As soon as the Range Extender is connected and has been detected, the cumulative charge is displayed on the interface. To view the charging status of the Range Extender on its own, press the button on the Range Extender, then the LEDs will display the charging status of the Range Extender.
Are there level shifters that I could mount on the handlebars?
Yes, there is a solution with two small buttons, for racing bikes, as well as a solution with a small rocker switch, primarily for MTB handlebars. Both solutions are cable-connected and can be retrofitted at any time.
Do you want to get in contact with the BIKEDRIVE team directly?
-> maxon's BIKEDRIVE & e-mobility contact form
Comments
0 comments
Article is closed for comments.