Motivation:
It is your first time to use "Motion Studio" and the ESCON2 and want to gather some information to get quickly into this new controller product line and its software tools.
What is the ESCON2?
The ESCON2 product line from maxon consists of compact, powerful 4-quadrant PWM servo controllers. Their high power density provides flexibility for use with brushed DC motors and brushless EC motors (BLDC) up to 1,800 W continuous power with various feedback options, such as Hall sensors, incremental encoders, and absolute encoders in a variety of drive applications. The ESCON2 servo controllers are specially designed for commanding and controlling on the basis of analog and digital set values and for use as slave nodes in a CANopen network. They also offer extensive analog and digital I/O functionality. The latest technologies, such as field-oriented control (FOC) and feed-forward acceleration/velocity control in combination with the highest cycle rates, enable sophisticated yet user-friendly motion control, even if the position sensor resolution is limited. The Motion Studio graphical user interface, available free of charge, enables fast configuration, convenient monitoring and analysis, and automated tuning of all drive systems.
Ready-to-connect units:
A variety of ready-to-connect controllers in various power classes and designs of the ESCON2 product line provide attractive economical options for easy integration in mechanical and equipment engineering.
Module, Micro, Nano:
Robotic, analysis, and handing systems require compact integration of a large number of energy-efficient drives, combined with highly dynamic controllers and a linked bus system. With the ESCON2 Modules, Micro and Nano, modular multi-axis systems can be set-up using CANopen without needing high investment in development.
ESCON2 features
- Very high power density
- Optimized efficiency
- Extensive I/O functionality
- Sinusoidal commutation (FOC)
- Current and velocity controller with high performance even if the position sensor resolution is limited (e.g. if just Hall sensors and no encoder are in use).
- Configurable protective functions for controller and drive
- I/O standalone mode or CANopen slave in accordance with CiA 301, 402, 305;
alternatively, can be configured and receive commands via USB or serial interface (RS232) - Easy to configure and commission with Motion Studio GUI
- All software components are available for free
- Full documentation
Video tutorials:
Please check the following linked video tutorials to setup "Motion Studio" and your ESCON2:
- Motion Studio: Getting started
- ESCON2 / Motion Studio: Configuration of a DC motor and its sensors
- ESCON2 / Motion Studio: Configuration of a brushless DC (= EC) motor and its sensors
- ESCON2 / Motion Studio: Regulation Tuning
- ESCON2 / Motion Studio: I/O Configuration
Do not miss to have a look into "Motion Studio User Guide.pdf" which is installed on your local drive:
-> C:\Program Files (x86)\maxon\Motor and Motion Control\Software\Motion Studio
Most important manuals:
- Take a look at the "Motion Studio User Guide.pdf" installed on your local drive:
-> C:\Program Files (x86)\maxon\Motor and Motion Control\Software\Motion Studio
-
For commissioning and wiring please refer to the “Hardware Reference” of your ESCON2 product type and for commanding via CANopen please refer to the “ESCON2 Firmware Specification.pdf”. All these technical manuals are installed on your local drive or can be downloaded from the corresponding maxon ESCON2 product page:
-> C:\Program Files (x86)\maxon\Motor and Motion Control\Manuals\ESCON2
A closer look at the ESCON2 highlights:
-
If you would like a brief overview of the most important features of the ESCON2, please refer to the attached document “2025-05_ESCON2-MagazineReport-EN_V1-10.pdf”.
-
If you would like to learn more about the details behind the highlights, please also read the comprehensive attached document “2025-01_ESCON2-WhitePaper-EN_V1-20.pdf”.
A quick overview of the ESCON2 product line:
- Please take a look at the attached document "ESCON2_ProductLine-Presentation_V1-00.pdf".
Cross reference:
Not sure what maxon controller product line is the best choice for your application's requirements? Have a look into the linked Support Center document:
-> "EPOS4, ESCON2, ESCON: What controller should I select?".
Assistance required?
Feel free to ask our experts of the local maxon sites or submit a support request.
- Click on the "Global" tab of the "A Global network" section of www.maxongroup.com/en/contact
or - Submit a support request and share as much information as possible about your application, its requirements, intended maxon and 3rd party components in use, and your focused point of discussion.
Comments
0 comments
Article is closed for comments.