This article describes the relationship between the different motor constants (e.g. speed and torque constant).
Generally, motor constants result from the construction details of a given motor. Such as
- active length and diameter
- winding geometry, winding resistance and winding number
- magnetic flux densities, permanent magnets
Torque constant kM
- relates the produced torque to the motor current
- maxon unit: mNm / A
- SI unit: Nm / A
Speed constant kn
- relates the motor speed to the back EMF voltage
- maxon unit: rpm / V
- SI unit: rad/s / V
Relationship between kn and kM
- kn is basically the inverse of kM
- in maxon units
- in SI units
Generator constant kG
- relates the generated back EMF voltage to the motor speed
- the inverse of the speed constant: kG = 1/ kn
- unit: V / rpm
- often also in V / 1000rpm
Motor constant k
- used to express the strength of the motortype (size)
- independent of the winding details, such as resistance R
- relation:
with:
-
- M = torque
- PJ = Joule power loss (= R * I2)
- The maxon speed-torque-gradient
is proportional to 1 / k2.
Comments
0 comments
Article is closed for comments.