Jürgen Wagenbach
- Total activity 548
- Last activity
- Member since
- Following 0 users
- Followed by 2 users
- Votes 2
- Subscriptions 408
Articles
Recent activity by Jürgen Wagenbach Sort by recent activity-
UL File Number
Topic: What is the meaning of an "UL File Number"? Where can the "UL File Number" be found by maxon documents? Solution: UL stands for "Underwriter Laboratories" and is an US certification author...
EPOS4 / IDX: Analog set value commanding
Topic:How to configure an EPOS4 or an IDX to command the speed or current control by an analog set value? Technical background:An analog set value can be used to command the "CSV - Cyclic Synchrono...
EPOS4: Commanding without a motor present?
Topic: How to configure the EPOS4 to get rid of error messages even if no motor and encoder is connected? Situation: A master's program flow and communication with EPOS4 has to be tested without ...
Windows'10: Uninstall EPOS Studio
Topic: How to uninstall EPOS Studio in case of Windows'10? Situation: If there is already an "EPOS Studio" version installed by your PC system, this one has to be unistalled before the "EPOS Setu...
CAN bus topology and bus termination
Topic: What has to be taken into account concerning a proper CAN bus wiring as the base of a reliable CAN bus communication? Solution: There are some important points which have to be taken into ac...
How to find the data sheet of a maxon product by its 6-digit part number?
Topic: How to find the data sheet of a motor, gear, encoder, or controller by its 6-digit part number on the maxon website? Solution: If you need some information about a maxon product with a 6-dig...
EPOS2 / EPOS4 / IDX: Commanding by Python -> pythonnet
Topic: Is it possible to command the EPOS4 (or EPOS2) by Python? Basics: maxon does not provide documentation, specific libraries, sample code, or support to command the EPOS controllers by Pytho...
ESCON: Digital Output Wiring
Topic: How to wire the digital outputs of an ESCON servo controller? What configuration features are available? Solution: The ESCON controllers provide two digital outputs. Different predefined f...
Warranty
maxon provides the statutory warranty of quality and title for all newly manufactured goods for a period of 12 months from passing of the risk. Repair or replacement shall not prolong the original ...
Parvalux PBL60 + maxon ESCON / EPOS4
Topic: How has a Parvalux / PBL60 motor to be connected to a maxon ESCON or EPOS controller? What configuration is required to operate the PBL60? Solution: Parvalux / PBL60 brushless DC motors ha...