Speed control with encoder
What minimum motor speed does maxon recommend for a speed control with encoder?
10...100 rpm, depending on the application.
The resolution of the encoders should be at least 500 counts per turn (revolution).
With higher resolutions, e.g. 5'000 counts per turn, speeds below 10rpm can be realized.
See also Encoder Selection Video
Comments
0 comments
Article is closed for comments.