Jürgen Wagenbach
- Total activity 548
- Last activity
- Member since
- Following 0 users
- Followed by 2 users
- Votes 2
- Subscriptions 408
Articles
Recent activity by Jürgen Wagenbach Sort by recent activity-
maxon BIKEDRIVE AIR: Video tutorial "Disassembly of a battery and drive unit"
This linked video tutorial shows the disassembly of maxon's BIKEDRIVE AIR battery and drive unit: Please visit maxon's BIKEDRIVE website for more questions about the maxon BIKEDRIVE AIR system and...
EPOS Studio Installation: Selection of supported product lines
Topic: What has to be checked during installation of "EPOS Studio"? Situation: If you have "EPOS Studio" installed and want to open a project or connect to an "EPOS", "EPOS P", or "MCD", it might...
ESCON EC-S: Applications and restrictions of sensorless control
Topic: Sensorless control of brushless motors (= EC motors) can be a quite attractive solution because there are no feedback sensors required. Finally this means less components in use and just the...
EPOS4: Sensors & start procedure of sinusoidal commutation
Topic: What kind of sensors are mandatory for a sinusoidal commutation? When does sinusoidal commutation become active during the inital movement? Situation: There are two different kinds of win...
EPOS Command Library: Data exchange rates?
Topic: Why is not possible to exchange data every 1 ms by USB (or other interfaces)? What data exchange cycle times can be achieved by using the EPOS Command Library? Remark: The term “EPOS” ref...
EPOS2 versus EPOS4: Connectors, Object Dictionary, Operating modes, Libraries
Topic: What has to be considered if an EPOS2 of an existing system should be replaced by an EPOS4 in future? Is it possible to use EPOS2 programming libraries also for EPOS4? Situation: You hav...