Topic:
- What means "Self-locking" or "Back-drivable"?
- How can it be judged if a gear or drive unit is "self-locking" or "back-drivable?
- For what types of applications get "Self-locking" or "back-drivable" an important aspect?
General important remarks:
- Any torque applied to a gear's output shaft has to be lower than the maximum torque specified by the gear's data sheet.
- Caution: Higher torques can damage the gear!
- Caution: Higher torques can damage the gear!
- Distinguish self-locking and back-drivability on the naked gearhead and on the complete(!) drive unit with gearhead, motor and maybe additional mechanical elements.
- The naked gearhead might be back-drivable while the complete unit is not.
- The naked gearhead might be back-drivable while the complete unit is not.
Solution:
1.) Self-locking gears resp. motor combination
1.a.) Meaning:
Self-locking means that when applying a torque to the gear's output shaft, it will not rotate and thereby is locked. Hence, self-locking always refers to a static situation.
1.b.) Special definitions
- Intrinsically self-locking
- This is a gear where the torque in the backward direction lies within the cone of friction whereas in the forward direction it is outside of it.
- Intrinsically self-locking gearheads cannot be moved by a steady force from the load. However, they may drift back if the gear is subject to vibrations.
- Typical intrinsically self-locking gears are worm gears or linear screw gears, when the forward efficiency is below 50%. However, planetary or spur gears, even with 5 stages are never intrinsically self-locking, although most of the time functionally self-locking.
- Among maxon gears, only the metric or trapezoidal screw drives are intrinsically self-locking.
- Functionally self-locking:
- In functionally self-locking drive units, the highest expected and permissible torque on the load side (breaking torque) is too low to overcome the friction and/or detent torque of the primary side.
- Functional self-locking properties are often achieved with 4 or 5-stage planetary gearheads.
However, it is difficult to really grant for this property in general.
1.c.) Applications
Self-locking is desirable in applications ...
- ... where the most common operation state is standstill (without power).
- ... that need to lift and/or hold loads against gravity or other constant external force
(e.g. crane applications or holding position in case of an emergency even if no brake is present). - ... where the costs of a braking system are to be saved.
1.d.) Additional notes
- Many drives with gears of higher reduction are functionally self-locking because the load is not able to overcome the primary friction and/or detent torque. However, it is difficult to really grant for this property in general.
- Functional self-locking properties are often achieved with 4 or 5-stage planetary gearheads.
- Functional self-locking properties are often achieved with 4 or 5-stage planetary gearheads.
-
Secure self-locking can however only be guaranteed for custom specific drive designs.
2.) Back-drivable gears resp. motor combinations
2.a.) Meaning
A gearhead is called back-drivable if it can be driven from the gearhead shaft side applying a torque that is smaller than the max. continuous torque (or max. intermittent torque). Hence, back-drivability is always meant for a dynamic situation.
2.b.) Back-drivable or not?
Whether a gear resp. motor combination can be back-driven or not depends on ...
-
... the gear's design type and its reduction ratio.
-
... the teeth geometry, which influences the friction and friction type. Pulling friction is dominant in forward direction and differs from pushing friction in backward direction.
-
... the mechanical play between gear's components and the tilting of floating gear stages.
-
... the gear's efficiency, which reflects the friction in the gear and the viscosity of the lubrication and its temperature dependency.
-
... the friction and cogging at the gear input, i.e., the motor friction
⇒ graphite brushes exhibit more friction than metal brushes
⇒ motors with iron core winding show cogging which can lead to increased self-locking
2.c.) Applications
Back-drivability is desirable in applications ...
- ... where the mechanism should be moved by hand in case of power loss or for maintenance reasons.
- ... where the drive is used as generator. The unit is constantly driven from the gear output.
- ... where robots work with humans (cobot).
- ... in which external forces must be estimated, e.g. contact forces of walking robots in unstructured environments (uneven ground).
2.d.) Additional notes
- maxon planetary gearheads are optimized for forward operation and not specially made to be back-driven.
Some rule of thumbs
- Units with standard planetary gearheads with 1 or 2 stages are generally considered back-drivable. It is just possible that the mechanical misalignment between motor and 1-stage gearheads might lead to a notchy behavior in forward direction and reduced back-drivability in backward direction.
- maxon planetary gear's with the remark "UP - Ultra Performance" are usually back-drivable due to their high efficiency.
- Planetary gearheads with 3 stages may or may not be self-locking or back-drivable.
- Planetary gearheads with 4-5 stages are typically rated as "functionally self-locking" within the permissible torque level unless there is some special back-drivable design present.
- A spur gearhead is always back-drivable. Even with more than 3 stages.
Cross Reference:
- maxon's training video: "Gearhead selection"
- maxon's catalog -> http://epaper.maxongroup.com
- "Technology short and to the point: maxon gear"
(Page 70/71 of catalog 2022/2023) - "Standard specification No. 102"
(Page 87 of catalog 2022/2023) - "Explanations of maxon terminology gear and screwdrive"
(Page 354 of catalog 2022/2023)
- "Technology short and to the point: maxon gear"
Comments
0 comments
Article is closed for comments.