Topic:
- Can a motor be operated with a higher controller's supply voltage than specified by the motor's "Nominal voltage"?
- Is there some risk that the motor winding gets damaged if a higher voltage than the specified motor's "Nominal voltage" is applied?
Solution:
The motor's "Nominal voltage" has no meaning about the voltage which can be applied to the motor winding or to the motor controller.
Please find the meaning of the "Nominal voltage" by "Explanations of maxon terminology EC motor" resp. "Explanation of maxon terminology DC motor" of maxon's catalog (-> http://epaper.maxongroup.com), e.g. by page 86, 90 or page 186 of maxon's catalog 2022/2023:
General notes:
- The controller adapts the motor voltage according to the commanded speed and controls the motor current according to the demanded motor torque to follow a position or speed command resp. profile.
A motor controller acts as a power converter, see also by this linked Support Center document:
-> Motor controllers: Input current versus Motor current, Power Conversion - A supply voltage of 24VDC or 48VDC or even 70VDC in case of higher rated ESCON or EPOS motor controllers will not harm or damage a motor specified for a lower "Nominal voltage" level.
- We recommend choosing a controller with a "Continuous output current" that roughly matches the "nominal current" of the motor.
The supply voltage of the controller is less (or even not so) important. Do not choose a power stage that is too oversized in terms of the nominal current of the power stage compared to the "nominal current" of the motor. - Take care that the supply voltage of the controller is sufficient to reach the commanded speed.
Please find some more information about this by the following linked Support Center document:
-> What supply voltage is required by a controller?
Finally this even means that the controller's supply voltage has to be higher than the specified motor's "Nominal voltage" if you want to reach the motor's "Nominal speed" (due to some motor data tolerance and voltage drop by the controller).
Conclusion:
A controller supply voltage of 24V or 48V are typically in use by most applications because this is the rating of most industrial power supplies too. The supply voltage of the controller must be high enough to reach the required motor speed. Don't worry, the controller ensures that the motor is not damaged.
Specific note concerning DC motor and direct supply:
A DC motor can be also operated by a supply voltage directly connected to the +/- cable of the motor (without any controller in between). In this case it has to be ensured that the supplied voltage does not result in a motor shaft speed (= approx. 'supply voltage' x 'speed constant) which exceeds the motor's "Max. speed" rating. 
If the "Max. speed" is exceeded, the service life of the motor is reduced. If the speeds are far too high, the motor can also be damaged (e.g. by an internal bearing or winding damage).
Comments
0 comments
Article is closed for comments.