What torque does the maxon BIKEDRIVE AIR e-bike system provide?
The system delivers a peak torque of around 30 Nm.
How many levels of support are there?
There are three levels of support. The manufacturer defines its factory settings, but the end customer can then make individual adaptations.
Can I configure the support levels myself?
Yes. With the maxon Connect app, the levels can be individually configured and saved. It is possible to revert to the factory settings at any time.
Do you want to get in contact with the BIKEDRIVE team directly?
-> maxon's BIKEDRIVE & e-mobility contact form
Comments
0 comments
Article is closed for comments.