# -*- coding: utf-8 -*-
"""
Example to command EPOS4 with python
Operation Mode: Profile Position Mode, 10cycles repeated
No Homing

Python Version 3.7
Tested with Raspberry Pi 3

Created on 24.02.2021
Version 1.0
@author: CCMC, maxon motor ag, Switzerland

"""

from ctypes import *

# sleep function
import time

# Folder created for example: /home/pi/src/python/
# Copy maxon motor Linux Library arm v7 into this folder
# Library must match according your cpu, eg. PI3 has arm v7
# EPOS Comand Library can be found here, when EPOS Studio has been installed:
# C:\Program Files (x86)\maxon motor ag\EPOS IDX\EPOS4\04 Programming\Linux Library
path='/home/pi/src/python/libEposCmd.so.6.6.2.0'
cdll.LoadLibrary(path)
epos=CDLL(path)

# Node ID must match with Hardware Dip-Switch setting of EPOS4
NodeID=1
keyhandle=0
# return variable from Library Functions
ret=0
pErrorCode=c_uint()
pDeviceErrorCode=c_uint()


## ============================================================================================
# Read Statusword and mask it to bit12
def WaitAcknowledged():
	ObjectIndex=0x6041
	ObjectSubindex=0x0
	NbOfBytesToRead=0x02
	pNbOfBytesRead=c_uint()
	pData=c_uint()
	pErrorCode=c_uint()

	# Setpoint Acknowledged
	Mask_Bit12=0x1000
	Bit12=0
	i=0

	while True:
		# Read Statusword
		ret=epos.VCS_GetObject(keyhandle, NodeID, ObjectIndex, ObjectSubindex, byref(pData), NbOfBytesToRead, byref(pNbOfBytesRead), byref(pErrorCode) )
		Bit12=Mask_Bit12&pData.value

		# Timed out
		if i>20:
			return 0
			break

		if Bit12==Mask_Bit12:
			time.sleep(1)
			i+=1

		# Bit12 reseted = new profile started
		else:
			return 1
			break



def CyclicMode(pErrorCode):

	print('Wait finishing positioning...')

	for x in range(1, 11):
		print('Loop: %d' % x)

		# TargetPosition=20'000qc / AbsolutMovement=0 =>Relative Positioning / StartProfileImmediately=0
		ret=epos.VCS_MoveToPosition(keyhandle, NodeID, 20000, 0, 0, byref(pErrorCode) )

		ret=WaitAcknowledged()

		# Send new profile during execution of previous profile
		ret=epos.VCS_MoveToPosition(keyhandle, NodeID, -20000, 0, 0, byref(pErrorCode) )

		ret=WaitAcknowledged()

	print('Cyclic movemenent finished')

	return 1



# Example of using VCS_GetObject()
# With this function any CANopen Object can be accessed
def GetPosition():
	# CANopen Object: Position Actual Value
	ObjectIndex=0x6064
	ObjectSubIndex=0x00
	NbOfBytesToRead=0x04
	# DWORD
	NbOfBytesRead=c_uint()
	# 0x6064 => INT32
	pData=c_int()
	pErrorCode=c_uint()

	ret=epos.VCS_GetObject(keyhandle, NodeID, ObjectIndex, ObjectSubIndex, byref(pData), NbOfBytesToRead, byref(NbOfBytesRead), byref(pErrorCode) )

	if ret==1:
		print('Position Actual Value: %d [inc]' % pData.value)
		return 1
	else:
		print('GetObject failed')
		return 0



# Get Position direct via function
def GetPositionIs():
	pPositionIs=c_long()
	pErrorCode=c_uint()

	ret=epos.VCS_GetPositionIs(keyhandle, NodeID, byref(pPositionIs), byref(pErrorCode) )

	if ret==1:
		print('Position Actual Value: %d [inc]' % pPositionIs.value)
		return 1
	else:
		print('GetPositionIs failed')
		return 0



## ============================================================================================
# Main
# Open USB Port
print('Opening Port...')
keyhandle=epos.VCS_OpenDevice(b'EPOS4', b'MAXON SERIAL V2', b'USB', b'USB0', byref(pErrorCode) )

if keyhandle != 0:

	print('Keyhandle: %8d' % keyhandle)

	# Verify Error State of EPOS4
	ret=epos.VCS_GetDeviceErrorCode(keyhandle, NodeID, 1, byref(pDeviceErrorCode), byref(pErrorCode) )
	print('Device Error: %#5.8x' % pDeviceErrorCode.value )

	# Device Error Evaluation
	if pDeviceErrorCode.value==0:

		# Set Operation Mode PPM
		ret=epos.VCS_ActivateProfilePositionMode(keyhandle, NodeID, byref(pErrorCode) )

		# Profile Velocity=500rpm / Acceleration=1000rpm/s / Deceleration=1000rpm/s
		ret=epos.VCS_SetPositionProfile(keyhandle, NodeID, 500, 1000, 1000, byref(pErrorCode) )

		# Read Position Actual Value with VCS_GetObject()
		ret=GetPosition()

		ret=epos.VCS_SetEnableState(keyhandle, NodeID, byref(pErrorCode) )
		print('Device Enabled')

		ret=CyclicMode(pErrorCode)

		ret=epos.VCS_SetDisableState(keyhandle, NodeID, byref(pErrorCode) )
		print('Device Disabled')

		# Other Option to Read Position
		ret=GetPositionIs()

	else:
		print('EPOS4 is in Error State: %#5.8x' % pDeviceErrorCode.value)
		print('EPOS4 Error Description can be found in the EPOS4 Fimware Specification')

	# Close Com-Port
	ret=epos.VCS_CloseDevice(keyhandle, byref(pErrorCode) )
	print('Error Code Closing Port: %#5.8x' % pErrorCode.value)

else:
	print('Could not open Com-Port')
	print('Keyhandle: %8d' % keyhandle)
	print('Error Openening Port: %#5.8x' % pErrorCode.value)