Dieses Support Center Dokument steht aktuell nur auf Englisch zur Verfügung!
Topic:
Autotuning results in some stable control but there seems to be still some oscillation present (e.g. due to differing friction).
- Is there some general rule present how autotuned parameters might be still possible to be improved or better adapted to a mechanical system by manual modifications (e.g. in case of some oscillation)?
Solution:
I.) Current control
In general, the current controller does not need to be modified when manually tuning the velocity or position controller.
- In case of slotted motors and especially with EC-i motors the aggressiveness of the autotuned current controller may be relatively low. In this case, if the user wants to increase the gains of the position and/or velocity controller, then it is recommended that they increase the current control gains (move the tuning slider to the right) beforehand.
II.) Single loop velocity control with lowpass filter
Initial action:
If observer was initially chosen, then switch to lowpass filter.
Next action steps:
1. Execute autotuning initially.
2. Feedforward parameter modification (during manual tuning):
- Write down feedforward values
= keep the autotuned feedforward values in mind to set the identical values after manual tuning is finished later on. - Set feedforward values to zero
3. Select your "manual tuning" strategy depending of your aim:
- If the controller is not aggressive enough (e.g. low frequency oscillations, large following error), define scaling factor “k” larger than 1 (suggestion: 2)
- If the controller is too aggressive (e.g. high frequency oscillations),
define scaling factor “k” between 0 and 1 (suggestion: 0.5)
4. Modify the autotuned parameters
- Multiply P-gain by k
- Multiply I-gain by k^2
- Multiply lowpass "Filter cutoff frequency" by k
(This value is just present and can be adjusted by FW >= 0x170 only!)
5. If control performance is not yet satisfying, return to step 3.
Otherwise restore values of feedforward gains and stop.
III.) Single loop position control
1. Execute autotuning initially.
2. Feedforward parameter modification (during manual tuning):
- Write down feedforward values
= keep the autotuned feedforward values in mind to set the identical values after manual tuning is finished later on. - Set feedforward values to zero
3. Select your "manual tuning" strategy depending of your aim:
- If the controller is not aggressive enough (e.g. low frequency oscillations, large following error), define scaling factor “k” larger than 1 (suggestion: 2)
- If the controller is too aggressive (e.g. high frequency oscillations),
define scaling factor “k” between 0 and 1 (suggestion: 0.5)
4. Modify the autotuned parameters
- Multiply P-gain by k^2
- Multiply I-gain by k^3
- Multiply D-gain by k
5. If control performance is not yet satisfying, return to step 3.
Otherwise restore values of feedforward gains and stop.
Additional notes:
- In general, the roles of the PID control gains may be described as follows:
- Proportional gain: The main workhorse.
- Integral gain: Compensates constant too low-frequency disturbances, but causes overshoot and oscillations if too large.
- Derivative gains: Compensates high-frequency disturbances, but causes vibrations if too large.
- In general, the feedforward gains do not need to be modified after autotuning.
- During manual tuning it is recommended to set the feedforward gains to zero because, in this way, the effect of the manual modifications is much easier to evaluate.
- Finally the initially autotuned (and kept in mind) feedforward values have to be set again after manual tuning are finished.
- By multiplying the gains by different powers of the scaling factor “k”, the balance between the gains is maintained.
- If autotuning fails and the user does not have an initial set of gains to work with, then they may follow a manual tuning algorithm like the one by Ziegler and Nichols.
Example:
EC45flat (P/N: 251601) + gear GP23C (P/N: 166931) plus some conveyor belt with strongly differing friction.
- Initial state after autotuning. The conveyor belt has some unsteady friction resulting in some unsteady oscillation.
If you want to reduce this oscillation, the gains have to be increased. - Applying some scaling of k = 2 to the gains based on the rules of "Single loop velocity control" above, i.e. P-gain = P-gain * 2, I-gain = I-gain x 4)
- Applying a scaling factor of k = 2 once more again:
The control error has become even smaller but now the system oscillates at a speed value of 0 rpm. Finally it will be the decision of the system designer whether the oscillation at 0 rpm can be tolerated (e.g. because the control might be disabled at 0 rpm anyway) or the control parameters of the manual tuning step before are satisfying for the application.
Kommentare
0 Kommentare
Zu diesem Beitrag können keine Kommentare hinterlassen werden.